• No : 20941
  • Release Date : 2018/08/22 16:25
  • Print

FR-HC2

Does the inverter stop when the SOF signal of the HC2 is turned ON?
Category : 

Answer

The internal transistor of the HC2 stops by turning on the SOF signal and stopping the converter. As a result, regenerative driving is not performed. However, the test run of the inverter with no load can be performed because the voltage output between P and N is not shut off. (Since the main circuit capacitor or others of the HC2 generates heat, the normal operation to which a load is applied cannot be performed.)
Product Name
Inverter, magnet motor drive
Product Category
Option
Series
Option