- No : 20948
- Release Date : 2018/08/22 16:25
-
Print
FR-HC2
Is the inverter reset when RES of the HC2 is turned ON?
- Category :
-
Answer
Because RSO (converter reset) of the HC2 is connected to RES of the inverter, the inverter is reset along with the HC2 reset. (Refer to the wiring diagram in the Instruction Manual.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- Option