• No : 20952
  • Release Date : 2018/08/22 16:25
  • Print

Anti-sway control

When a swinging frequency is set in Pr.1074, do the setting values in Pr.1077 to Pr.1079 affect the control?
Category : 

Answer

No, it does not affect the control. When a swinging frequency is set in Pr.1074, the setting values in Pr.1077 to Pr.1079 are not referred. When Pr.1074 is set to "9999", the setting values in Pr.1077 to Pr. 1079 are referred.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800