• No : 20953
  • Release Date : 2018/08/22 16:25
  • Print

Anti-sway control

It is describes that when Pr.1074 is set to "9999", the anti-sway control is performed using a swinging frequency estimated by the inverter according to the settings of Pr.1077 to Pr.1079. When the load weight is 1 to 5 kg, what value should I set?
Category : 

Answer

Set 3 kg (intermediate value) for the load weight 1 to 5 kg.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800