- No : 20958
- Release Date : 2018/08/22 16:25
- 
          
              Print
          
        
 
Storage area
    
      It is described that the parameters for the PLC function and sequence programs are written to the flash memory and the number of writing times is limited (about 1,000,000 times). Is this storage area different from that of the EEPROM for the parameters of the inverter? 
    
  
    - Category : 
- 
      
    
 
    Answer
  
    The storage areas for the sequence programs and for the parameters of the inverter are different. 
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-A800, FR-F800