• No : 20961
  • Release Date : 2018/08/22 16:25
  • Print

Parameter copy to the USB memory

Can I read parameters to the USB memory during operation?
Category : 

Answer

Yes. Parameters can be read except during an inverter reset or when the password function is set.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800