- No : 20975
- Release Date : 2018/08/22 16:25
-
Print
FR-A800-CRN
It is described that the environmental resistance was improved. What does it mean?
- Category :
-
Answer
The inverter with circuit board coating (conforming to IEC60721-3-3 3C2/3S2) ensures reliability even in poor environments. Furthermore, the inverter with plated conductor is also available.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800