• No : 20977
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800

Though the control circuit temperature can be monitored with Pr.52=98, is any alarm generated when the control circuit temperature rises?
Category : 

Answer

No alarm occurs due to the abnormal temperature. In the main circuit, alarms such as heatsink overheat will be occurred.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800