• No : 20995
  • Release Date : 2018/08/22 16:25
  • Print

Output signal

Are there any restrictions on the wiring length of the output terminal RUN and relay terminal ABC?
Category : 

Answer

The length within 30 m is recommended. When the wiring length is long, signals may not be received accurately due to the increased inductance.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800, FR-D700, FR-E700, FR-E700EX