• No : 21001
  • Release Date : 2018/08/22 16:25
  • Print

MM-FR-A800

What is the minimum frequency of the point table positioning with the MM-CF?
Category : 

Answer

If the command is 0.01 Hz or higher, the positioning control is performed.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800