• No : 21013
  • Release Date : 2018/08/22 16:25
  • Print

Parameter copy to the USB memory

Can I write the USB memory parameter copy file (*.cp1) to the inverter when the power supply specification or capacity is different (such as when replacing the FR-A820 with FR-A840)?
Category : 

Answer

Yes. Writing is available when the power supply specification or capacity is different. Note that setting values of the voltage relation is also overwritten according to the voltage difference (200 V/400 V).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800