• No : 21017
  • Release Date : 2018/08/22 16:25
  • Print

Use of the DC reactor

Can I use the DC reactor supplied with the FR-A500L/FR-F500L for the FR-A800/F800?
Category : 

Answer

It can be used in terms of the specifications. However, it is recommended to update the reactor and inverter at the same time because the DC reactor was manufactured over ten years ago.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800