• No : 21018
  • Release Date : 2018/08/22 16:25
  • Print

Control power supply

Can I use separate power supply for the control circuit with the 24 V external power supply?
Category : 

Answer

Turning ON the main circuit power stops the 24 V external power supply operation and enables the normal operation. Therefore, the separate power supply cannot be used with the 24 V external power supply. Use the power supply terminal for control circuit (R1/L11, S1/L21) for using the separate power supply. (For the detail, refer to the Instruction Manual.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800