- No : 21021
- Release Date : 2018/08/22 16:25
-
Print
Frequency setting increment
When the setting frequency increments and monitor increments are set to 0.1 rpm with Pr.811 = 1, why is the value displayed in 1 rpm increments after monitoring?
- Category :
-
Answer
The value is displayed in 0.1 rpm increments under Vector control. However, the value is rounded down to the first decimal place and displayed in 1 rpm increments under other control methods.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800