• No : 21022
  • Release Date : 2018/08/22 16:25
  • Print

Vector control

When the setting of Pr.83 and Pr.84 are enabled? When Pr.71 is set to "30" (Vector control dedicated motor) under Vector control, why is the output voltage not changed by changing Pr.83?
Category : 

Answer

Both settings of Pr.83 and Pr.84 are enabled immediately. However, the output voltage is not changed because the value of Pr.83 has little influence on Vector control. Since the output voltage is calculated from the motor constant, the output voltage is when the motor constant is changed by executing the tuning.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800