- No : 21023
- Release Date : 2018/08/22 16:25
-
Print
JIS standard
Is the inverter compliant with the JIS standard?
- Category :
-
Answer
JIS standard for the inverter is not established. It is required to check whether the whole machine including the inverter is compliant with JIS standard.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800, FR-D700, FR-E700, FR-E700EX