• No : 21058
  • Release Date : 2018/08/22 16:25
  • Print

Simple magnetic flux vector control

When Pr.80 and Pr.81 are set, the simple magnetic flux vector control is used in the FR-F700P; however, the advanced magnetic flux vector control is used in the FR-F800 instead. Is the simple magnetic flux vector control not available for the FR-F800?
Category : 

Answer

The simple magnetic flux vector control is unavailable for the FR-F800. The advanced magnetic flux vector control is higher-level function of the simple magnetic flux vector control. Thus, the advanced magnetic flux vector control is used in the FR-F800.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-F800