• No : 21059
  • Release Date : 2018/08/22 16:25
  • Print

FR-A842

Is the inrush current limit circuit built in the FR-A842? If it is not built in, is there any problem combining it with the FR-HC2?
Category : 

Answer

The inrush current limit circuit is not built in the FR-A842 (inverter unit). It is built in the FR-CC2 (converter unit), which is combined with the FR-A842. There is an inrush current limit circuit in the outside box of the FR-HC2. Thus, there is no problem for combining the FR-A842 with the FR-HC2. When the FR-HC2 is used, the FR-CC2 is not required.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800