- No : 21070
 
      - Release Date : 2018/08/22 16:25
 
        - 
          
              Print
          
        
 
  
 
The number of input terminals
    
      Is the number of input terminals the same as that of the F700P series? 
(For F700P: STF, STR, STOP, RH, RM, RL, JOG, RT, MRS, RES, AU, CS)
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    The number of terminals: There are the same input terminals as F700P and the following terminals (4 points) are added. Safety: SI1, SI2, SIC 24 V power supply: + 24 *The terminals SI1, SI2, and SIC are dedicated to the safety. Functions cannot be changed as other terminals.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-F800