• No : 21074
  • Release Date : 2018/08/22 16:25
  • Print

24 VDC power supply

To input the power supply of the control circuit from the 24 V external power supply, should I remove the jumper of the R1 and S1?
Category : 

Answer

Do not remove the jumper of the R1 and S1 when inputting the control circuit power supply from the external 24 V power supply (connecting across the terminals +24 and SD). Remove the jumper when using the separate power supply (200 V/400 V) for the control circuit.* The external 24 V power supply operates as a control power backup when the main circuit power supply is OFF. Thus, the external 24 V power supply is OFF when the main circuit power supply is used.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800