- No : 21085
- Release Date : 2018/08/22 16:25
-
Print
Auto tuning
Is the capacity of the motor that can be handled by auto tuning the same as or one rank lower similarly to the A700?
- Category :
-
Answer
The 800 series supports the multiple rating. Thus, the rated current of the corresponding motor is 40% or higher of the inverter rated current. (Using a motor with the rated current substantially lower than the rated inverter current will cause torque ripples, etc. and degrade the speed and torque accuracies.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800