• No : 21094
  • Release Date : 2018/08/22 16:25
  • Print

EMC filter

Is an EMC filter built in?
Category : 

Answer

A capacitive filter and common mode choke are built in. (A common mode choke is built in only for the 55K or lower.) Use a connector for whether to turn ON or OFF the capacitive filter. In the initial setting, the capacitive filter is set to OFF.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800