• No : 21096
  • Release Date : 2018/08/22 16:25
  • Print

USB version

What is the USB version?
Category : 

Answer

Ver1.1 (Ver2.0 (full speed) compatible). USB1.1 supports Full Speed (12 Mbps) and Low Speed (1.5 Mbps) transmission speed modes. USB2.0 supports High Speed (480 Mbps), Full Speed (12 Mbps), and Low Speed (1.5 Mbps) transmission speed modes. USB2.0 is compatible with USB1.1, and the both support Full Speed. The A800/F800 series can open communication at Full Speed.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800