• No : 21099
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800

Is the number of input terminals the same as that of the A700 series?
(For A700: STF, STR, STOP, RH, RM, RL, JOG, RT, MRS, RES, AU, CS)
Category : 

Answer

Number of terminals: Same input terminals as the A700 series, and the following two terminals are added. Safety: SI1, SI2, SIC 24 V power supply: +24 * The terminals SI1, SI2, and SIC are dedicated to the safety. The function cannot be changed as other terminals.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800