• No : 21103
  • Release Date : 2018/08/22 16:25
  • Print

PLC function

Does the PLC function have the performance equivalent to that of typical programmable controllers?
Category : 

Answer

The processing speed, scan time, and others are slower than those of the programmable controllers. There are some restrictions in the number of I/O points, program capacity, number of instructions, and others. For the detail, refer to the Instruction Manual.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800