- No : 21121
- Release Date : 2018/08/22 16:26
-
Print
FR-A7NF
Can the automatic restart after instantaneous power failure function be used in FL network communication?
- Category :
-
Answer
Yes, it can. When the FR-A7NF is installed, the CS terminal is disabled. Assign the CS terminal function to other input terminals by setting the parameter. By setting Pr.178 (STF terminal function) to "6", or Pr.179 (STR terminal function) to "6", the CS terminal function can be assigned.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option