• No : 21147
  • Release Date : 2018/08/22 16:26
  • Print

FR-HC2

What is the cable gauge of the inrush current limit resistor (FR-HCR2) of the FR-HC2?
Category : 

Answer

It is 0.88 mm2 (AWG18), and 0.3 mm2 (AWG24) for the thermostat.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
Option