- No : 21148
- Release Date : 2018/08/22 16:26
-
Print
FR-HC2
What happens when the FR-DU07 provided with the inverter is used for FR-HC2?
- Category :
-
Answer
It is not available and "Err" is displayed. When the FR-HC2 dedicated DU (FR-DU07-CNV) is installed to the inverter, "Err" is displayed as well. The FR-PU07 can be used with the FR-HC2 and inverter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- Option