- No : 21157
- Release Date : 2018/08/22 16:26
-
Print
FR-CV
Is there any problem with the ticking reactor FR-CVL?
- Category :
-
Answer
The reactor generates a sound during power regeneration, but it is not abnormal. [Reason] The noise from the reactor is caused mainly by the magnetic attractive force and magnetostrictive vibration at the iron core gaps, and magnetostrictive vibration of the silicon copper plate, which are transmitted to the iron core, generating a vibration sound come along with the resolution or reflection.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- Option