- No : 21194
- Release Date : 2018/08/22 16:26
-
Print
FR Configurator
Can the data saved by the Japanese version of FR-SW3 imported to the English version of FR-SW3?
- Category :
-
Answer
The parameter file (extension: pr3) can be imported. The system file (extension: mel) cannot be imported.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700