- No : 21205
- Release Date : 2018/08/22 16:26
-
Print
Remote setting function
In the Instruction Manual, it is described that "The remote setting function is disabled during JOG operation and PID control operation". Does the multi-speed function operate during JOG operation (or during PID control operation) with Pr.59 (Remote function selection) set 1 to 3?
- Category :
-
Answer
Because the multi-speed terminal is disabled, it does not operate in multi-speed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700