- No : 21206
- Release Date : 2018/08/22 16:26
-
Print
EEPROM writing with the communication option
Is the writing on the operation panel written to RAM when Pr.342 (Communication EEPROM write selection) is set to 1 with the communication option?
- Category :
-
Answer
The writing from the parameter unit or operation panel is always ROM write regardless of the setting value of Pr.342.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700