- No : 21212
- Release Date : 2018/08/22 16:26
-
Print
FR-HC2
Why did you start to recommend the fuse from the HC2? Can I use the breaker?
- Category :
-
Answer
It is fundamentally the same as the conventional model. Considering the recent safety awareness growth, we decided to start supporting it from the FR-HC2. Because the response speed of the breaker is slower than that of the fuse, the breaker cannot be used.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- Option