- No : 21221
- Release Date : 2018/08/22 16:26
-
Print
Communication EEPROM write selection (Pr.342)
This is related to 1 (write only to RAM) of Pr.342 (Communication EEPROM write selection). In the Instruction Manual, it is described that the changes of parameters are cleared when the power supply of the inverter is shut off. What happens when the reset signal is turned ON?
- Category :
-
Answer
They are cleared by the RES signal from the external terminals or inverter reset from the communication.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700