• No : 21368
  • Release Date : 2018/08/22 16:27
  • Print

Countermeasure against the instantaneous power failure with the inverter

As the countermeasure against the instantaneous power failure with the small type inverter (current model of the FR-A024 and A044), can I supply the power to the control power supply separately?
Even only for the control without operation, is the UPS available?
Category : 

Answer

The power cannot be supplied to the control power supply separately for the FR-A024/A044 and small type FR-E500.
Therefore, the UPS is not available.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A024, FR-E500