- No : 21368
- Release Date : 2018/08/22 16:27
-
Print
Countermeasure against the instantaneous power failure with the inverter
As the countermeasure against the instantaneous power failure with the small type inverter (current model of the FR-A024 and A044), can I supply the power to the control power supply separately?
Even only for the control without operation, is the UPS available?
- Category :
-
Answer
The power cannot be supplied to the control power supply separately for the FR-A024/A044 and small type FR-E500.
Therefore, the UPS is not available.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024, FR-E500