- No : 21369
- Release Date : 2018/08/22 16:27
-
Print
Vector control of the inverter
Under Advanced magnetic flux vector control, what happens with the speed fluctuation ratio with/without encoder?
- Category :
-
Answer
The speed fluctuation ratio under Advanced magnetic flux vector control of the FR-A500 is as follows.
Without encoder: ±1% With encoder (with A5AP): ±0. 02 % (at power driving load)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500