• No : 21397
  • Release Date : 2018/08/22 16:27
  • Print

Thermal protection

When the optional FR-ABR high-duty brake resistor is installed, is it necessary to provide thermal protection?
I think this is necessary to prevent fire that may occur when the transistor inside the inverter explodes and the resistor temperature goes abnormally high. Am I correct?
Category : 

Answer

Providing thermal protection is better for your safety.
When the brake transistor explodes, the brake transistor alarm (E.BE) is output. Consider a countermeasure using this signal to shut off the inverter power supply.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A024