• No : 21410
  • Release Date : 2018/08/22 16:27
  • Print

Installing reactor for suppressing harmonics

The catalog explains that one reactor needs to be installed on each inverter. Is it possible to install a reactor on one inverter and connect multiple inverters to the first inverter's output side?
If it is possible, does this configuration conform to the harmonic suppression guidelines for household appliances and general-purpose products?
Category : 

Answer

You can connect multiple inverters to a single reactor.
In this case, the load seems to be light from the reactor unless all of the inverters are rotating and the power factor improving effect is lowered.
It cannot be judged whether or not this configuration conforms to the harmonic suppression guidelines for household appliances and general-purpose products because this configuration is not covered. However, as mentioned above, the power factor improving effect (harmonics reduction effect) can be obtained as described in catalog when all inverters are operating, this configuration is considered to be acceptable.
Product Name
Inverter, magnet motor drive
Product Category
Power factor improving reactor
Series
Option