• No : 21414
  • Release Date : 2018/08/22 16:27
  • Print

EMC countermeasure

Let me know precautions when exporting equipment using the inverter to the United Kingdom, U.S.A., or Canada.
Category : 

Answer

To conform to the EMC Directive when exporting to an EU country, install the filter that conforms to the EMC Directive on the inverter, and take measures according to Mitsubishi "EMC guidelines".
Note that the entire equipment with the inverter built in must conform the to the EMC Directive.
When exporting to U.S.A. or Canada, power drive devices for industrial application such as inverters are not subject to the EMC regulation (FCC and others) and there is no special precaution regarding EMC.
Our inverter products have acquired the UL and cUL certification.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A500