- No : 21427
- Release Date : 2018/08/22 16:27
-
Print
Indication of potentiometer on operation panel
When I raise the frequency using the potentiometer on the operation panel, indication stops at 61.12.
How can I raise it (up to around 90.00)?
- Category :
-
Answer
The potentiometer on the operation panel is initially calibrated so that the maximum indication is slightly over 60 Hz with the potentiometer turned to the maximum position.
You need to calibrate Pr.923 so that it indicates 90 Hz at the maximum position.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500