- No : 21434
- Release Date : 2018/08/22 16:27
-
Print
Motor characteristics at low input voltage
I use the FREQROL-V200 with the dedicated motor (rated at 400 V) at the input voltage of 380 V.
Your catalog explains that the output voltage in this case will be 380 V. What about the motor rating?
Are the rated torque and output reduced?
- Category :
-
Answer
Since the dedicated motor is designed with the rated voltage of approximately 320 V, it can produce sufficient torque for the input voltage of 380 V.
Therefore, you can use it at the rated torque and output.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Dedicated motor
- Series
- FR-V200