• No : 21449
  • Release Date : 2018/08/22 16:27
  • Print

Meaning of OL display

"OL" is displayed on the operation panel. What does it mean?
Category : 

Answer

"OL" stands for "overload".
Whenever current of 150% or more of the inverter rated current flows, "OL" is ON.
If you continue operation with "OL" is displayed, a thermal trip is triggered. Therefore you need to reduce the load.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200