- No : 21468
- Release Date : 2018/08/22 16:27
-
Print
Difference between use with A100 and other types
I use the FR-BLF line noise filter.
The list of options on the catalog explains that two or more filters should be used when the wire is too thick to cover with a single filter for the A100. However, it instructs to use four or more filters for the A200 or A500.
Can I use four filters also for the A100?
Or, is it OK to use fewer filters for the A100 considering the relationship with the inverter?
- Category :
-
Answer
Similarly to the FR-A200 and A500, four or more filters should be used also for the FR-A100.
In short, it is OK if the wire penetrates the filter four times. (For certain wire sizes, two filters will do by winding the wire around the filter two times.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Noise filter
- Series
- Option