- No : 21471
- Release Date : 2018/08/22 16:27
-
Print
Inverter operation against power supply voltage drop
If the power supply voltage drops to 60% to 70% level in approximately 50 to 100 ms, how does the inverter (A500) operate?
- Category :
-
Answer
Depending on the load current, undervoltage protection (UVT) or instantaneous power failure protection (IPF) is triggered to shut off the inverter output, and the (inverter) trips. (Reset the inverter to restart it.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500