- No : 21523
- Release Date : 2018/08/22 16:28
-
Print
Amount of heat
How much heat does the inverter (FR-A520-5.5K) itself generate?
The load is the main shaft of a 3.7 kW 4P standard motor for approximately 50% continuous operation.
- Category :
-
Answer
The inverter (FR-A520-5.5K) itself generates approximately 310 W of heat.
This is the amount generated under the inverter rated current 100% load.
Since the load in your case is 3.7 kW and the amount of heat generated is considered to be less than the above amount.
If you are planning to build the inverter into an enclosure, it is recommended to use the above value.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500