• No : 21550
  • Release Date : 2018/08/22 16:28
  • Print

Analog signal resolution

How are the internal processing speed and analog input signal resolution of the FR-A500 series compared with the servo MR-H series amplifier?
What about the FR-E500 series?
Category : 

Answer

The internal processing speed is not published.
The analog input specifications are as follows:
FR-A500???1/4000FR-E500???1/1000MR-H???1/4000
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500, FR-A500