- No : 21551
- Release Date : 2018/08/22 16:28
-
Print
Faults history upon power failure
I heard that the FR-A500 is reset when an instantaneous power failure of 100 msec or longer occurs and fault output is not performed. Is this event stored in the history data?
Or, is it not recognized as a fault?
- Category :
-
Answer
When an instantaneous power failure of 100 msec or longer occurs, the inverter is reset* and it is not recognized as a fault.
Since it is not recognized as a fault, it is not stored in the history data.
* Our perception is that power failure of 100 msec or longer is not an instantaneous power failure but a normal power off (for example, MCCB OFF).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500