- No : 21565
- Release Date : 2018/08/22 16:28
-
Print
Inverter selection when multiple inverters are to be connected
When multiple inverters are to be connected, how should I choose them?
- Category :
-
Answer
Be sure to use a high power factor converter with the capacity higher than the total capacity of the inverters connected. (Note: One or more of the inverters must have capacity more than half of the high power factor converter.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option