- No : 21569
- Release Date : 2018/08/22 16:28
-
Print
Combination with existing inverters
Can it be combined with the existing inverters?
- Category :
-
Answer
Since the existing inverters do not have a terminal to connect to the FR-HC, it cannot be connected to them.
Use an inverter compatible with the high power factor converter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option